LTE FDD

Carrier Settings ARB

This topic describes carrier settings for Waveform Playback (ARB) capability. Settings are unique for each selected component carrier.

The SCPI mnemonic CCARrier<n> denotes CCARrier[1]|2|…|<n> where <n> is the number of configured carriers.

General

Enabled

Waveform Generation Length Even Frame Alignment

Waveform Generation Length

Carrier Type

Baseband

Auto Oversampling Ratio

Oversampling Ratio

Base Sampling Rate

Total Sample Points

Frequency Offset

Power

Timing Offset

Initial Phase

Spectrum Control

Pre-Filter Clipping

Post-Filter Clipping

Auto Symbol Rolloff Length Configuration

Symbol Rolloff Length

Baseband Filter

ACP Optimized Filter Type

Carrier Aggregation

Auto Carrier Aggregation Configuration

Primary Cell

Uplink

Downlink

PRACH

Carrier Configuration Tools

General

Enabled

This setting specifies the enable state of a carrier.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>[:STATe]?

SCPI Example

:RAD:LTEF:WAV:CCAR OFF

:RAD:LTEF:WAV:CCAR?

State Saved

Yes

Preset

ON

Initial S/W Revision

A.14.00

Waveform Generation Length Even Frame Alignment

[Uplink NB-IoT]

Double-click or use the drop-down menu to turn Waveform Generation Length Even Frame Alignment on or off.

SCPI Command

[SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier:LENGth:EVEN ON|OFF|1|0

[SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier:LENGth:EVEN?

SCPI Example

 

State Saved

Yes

Preset

ON

Waveform Generation Length

[Uplink E-UTRA/Uplink eMTC/PRACH E-UTRA/Prach NB-IoT/Uplink NB-IoT/Downlink NB-IoT]

Set the waveform generation length.

Waveform Generation Length must be a multiple of NPRACH Resource Periodicity on the Channel Setup node and the input value is rounded up to the nearest multiple of NPRACH Resource Periodicity.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:LENGth <time>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:LENGth?

SCPI Example

:RAD:LTEF:WAV:CCAR:LENG 20

:RAD:LTEF:WAV:CCAR:LENG?

State Saved

Yes

Preset

10 ms

20 ms [for Uplink NB-IoT/ Downlink NB-IoT]

When NB-IoT-NPRACH is selected then initially it is set to 80 ms. The Preset value, however, is 10 ms.

Min

10 ms

Max

30720 ms [Uplink E-UTRA/Uplink eMTC]

10240 ms [PRACH E-UTRA]

47360 ms [Uplink NB-IoT]

40960 ms [NB-IoT NPRACH / Downlink NB-IoT]

Resolution

1 ms [Uplink E-UTRA/Uplink eMTC]

10 ms [PRACH E-UTRA]

1 ms [Uplink NB-IoT]

10 ms [Downlink NB-IoT]

Initial S/W Revision

A.14.00

Modified S/W Revision

A.19.00

Carrier Type

This setting returns the carrier type. This setting is automatically set when a carrier is added.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:TYPE?

SCPI Example

:RAD:LTEF:WAV:CCAR:TYPE?

Notes

SCPI only, Query only

Returns FDDULEUTRA|FDDPRACHEUTRA|CW| FDDPRACHNIOT|FDDULNIOT

State Saved

No

Preset

FDDULEUTRA

Range

Uplink E-UTRA | PRACH E-UTRA | Continuous Wave| Uplink NB-IOT | Prach NB-IOT

Initial S/W Revision

A.14.00

Modified S/W Revision

A.19.00

Baseband

The parameters in the Baseband group set the baseband settings of a carrier.

Auto Oversampling Ratio

Sets the mode of oversampling rate control.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:OSRatio:AUTO[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:OSRatio:AUTO[:STATe]?

SCPI Example

:RAD:LTEF:WAV:CCAR:OSR:AUTO ON

:RAD:LTEF:WAV:CCAR:OSR:AUTO?

State Saved

Yes

Preset

ON

Initial S/W Revision

A.14.00

Oversampling Ratio

[Uplink E-UTRA/eMTC/Uplink NB-IoT/Prach-NB-IoT]

Sets the oversampling ratio of waveform generation.

This setting is available and used when Auto Oversampling Ratio is set to Off.

If Auto Oversampling Ratio is set to On, the signal generator automatically sets an optimized oversampling ratio for the current setup.

Double-click to set the oversampling ratio.

The Total Sample Points value is automatically determined based on the oversampling ratio. Using a larger oversampling ratio result in a more completely filtered image, but also uses more waveform memory by increasing the number of waveform points.

In Uplink E-UTRA/eMTC: In the case where the System Bandwidth = 1.4 MHz, Auto = 2, else Auto = 1.

In Uplink NB-IoT, Prach NB-IoT: System Bandwidth is 200 kHz Choices: AUTO | 1 | 2 | 3 | 4 | 5 | 6 | 7 Default: AUTO

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:OSRatio <integer>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:OSRatio?

SCPI Example

:RAD:LTEF:WAV:CCAR:OSR 2

:RAD:LTEF:WAV:CCAR:OSR?

Dependencies

This value is used when Auto Oversampling Ratio is Off.

State Saved

Yes

Preset

2

When Auto Oversampling Ratio is OFF, then Oversampling Ratio is 1.

Min

1

Max

7

Initial S/W Revision

A.14.00

Modified S/W Revision

A.19.00

Base Sampling Rate

[Uplink E-UTRA/eMTC][PRACH]

Base Sampling Rate is a sampling rate without Oversampling Ratio (OSR).

There is a relation among Base Sampling Rate, OSR, Total Sample Points, and Waveform Generation Length as follows.

Total Sample Points = Base Sampling Rate (MHz) x OSR x 1000 x Waveform Generation Length (ms)

Example: System BW = 5MHz, OSR = 1 (Auto), Waveform Generation Length = 10 (ms) case:

Total Sample Points = 7.68 (MHz) x 1 x 1000 x 10 (ms) = 76800 (Points)

The software sets the Base Sampling Rate based on the System Bandwidth (BW) as follows:

System BW = 1.4 MHz, Base Sampling Rate = 1.92 MHz.

System BW = 3 MHz, Base Sampling Rate = 3.84 MHz.

System BW = 5 MHz, Base Sampling Rate = 7.68 MHz.

System BW = 10 MHz, Base Sampling Rate = 15.36 MHz.

System BW = 15 MHz, Base Sampling Rate = 23.04 MHz.

System BW = 20 MHz, Base Sampling Rate = 30.72 MHz.

[Uplink E-UTRA/eMTC]

When Carrier Aggregation has multiple E-UTRA carriers or E-UTRA carrier of 15 MHz System Bandwidth and NB-IoT carrier(s), the Base Sampling Rate = 30.72 MHz.

[PRACH]

For multi-carrier waveforms, the Base Sampling Rate = 30.72 MHz.

[Uplink NB-IoT]

Displays Base Sampling Rate for each System BW or multi-carrier condition.

When System BW is 200 kHz, Base Sampling Rate is 1.92 MHz.

Example: System BW = 200 kHz, OSR = 1 (Auto), Waveform Generation Length = 20 (ms) case:

Total Sample Points = 1.92 (MHz) x 1 x 1000 x 20 (ms) = 38400 (Points)

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:SRATe:BASE?

SCPI Example

:RAD:LTEF:WAV:CCAR:SRAT:BASE?

Notes

Query only

State Saved

No

Preset

  • 15.36 MHz [Uplink E-UTRA/eMTC] [PRACH]

  • 1.92 MHz [Uplink NB-IoT]

  • 240 kHz [Prach NB-IoT]

Range

Value

1.92 MHz

3.84 MHz    

7.68 MHz    

15.36 MHz    

23.04 MHz    

30.72 MHz    

1.92 MHz

240 kHz

SCPI

F1M92

F3M84

F7M68

F15M36

F23M04

F30M72

Uplink NB-IoT

Prach NB-IoT

Initial S/W Revision

A.14.00

Modified S/W Revision

A.19.00

Total Sample Points

View the waveform length, displayed in points. You cannot edit this cell.

Total Sample Points is directly related to the Oversampling Ratio value selected. Increasing the oversampling ratio increases the total sample points.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:SAMPles:COUNt?

SCPI Example

:RAD:LTEF:WAV:CCAR:SAMP:COUN?

Notes

Query only

State Saved

No

Preset

153600

Initial S/W Revision

A.14.00

Frequency Offset

[Uplink E-UTRA/eMTC]

Sets the frequency offset for the carrier relative to the signal generator’s frequency setting.

The range of the parameter is coupled to the Oversampling Ratio, the Base Sampling Rate, the System Bandwidth and the max ARB Sample Clock of the connected signal generator.

Frequency Offset and Cell ID are always editable, even if Auto Carrier Aggregation Configuration is on.

In either case below (1 or 2), auto configuration is performed for Frequency Offset and Cell ID.

  1. When any of these actions are performed: Add Carrier, Delete Carrier or Change System BW, and the Auto Carrier Aggregation Configuration parameter is on.

  2. When the Auto Carrier Aggregation Configuration parameter is changed from off to on.

Auto configuration sets Cell ID same as Component Carrier Index.

If Auto Carrier Aggregation Configuration is set to off, auto configuration does not work.

[PRACH]

Sets the frequency offset for the carrier relative to the signal generator’s frequency setting.

The range of the parameter is coupled to Oversampling Ratio, Base Sampling Rate, System Bandwidth and the max ARB Sample Clock of the connected signal generator.

Frequency Offset is always editable, even if Auto Carrier Aggregation Configuration is on.

In either case below (1 or 2), auto configuration is performed for Frequency Offset.

  1. When any of these actions are performed: Add Carrier, Delete Carrier or Change System BW, and the Auto Carrier Aggregation Configuration parameter is on.

  2. When the Auto Carrier Aggregation Configuration parameter is changed from off to on.

If Auto Carrier Aggregation Configuration is set to off, auto configuration does not work.

[Uplink NB-IoT]

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:FREQuency:OFFSet <freq>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:FREQuency:OFFSet?

SCPI Example

:RAD:LTEF:WAV:CCAR:FREQ:OFFS 1000000

:RAD:LTEF:WAV:CCAR:FREQ:OFFS?

State Saved

Yes

Preset

0 Hz

Initial S/W Revision

A.14.00

Modified S/W Revision

A.19.00

Power

Sets the power level in dB for the selected carrier in a multiple carrier configuration, relative to the power settings defined for the other carriers in the configuration.

You can ignore this parameter for single carrier configurations.

In single carrier configurations, the amplitude of the signal is determined by the Amplitude setting in the Instrument node.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:POWer <rel_ampl>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:POWer?

SCPI Example

:RAD:LTEF:WAV:CCAR:POW -30dB

:RAD:LTEF:WAV:CCAR:POW?

State Saved

Yes

Notes

Unit in GUI: dB

Preset

0 dB

Min

-60 dB

Max

0 dB

Resolution

0.001 dB

Initial S/W Revision

A.14.00

Timing Offset

Specifies the length of timing offset.

The maximum value of the range depends on Waveform Generation Length.

If Timing Offset cannot be divided by sampling period (1 / Base Sampling Rate / Oversampling Ratio), it is rounded to the nearest sample point.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:TIMing:OFFSet <time>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:TIMing:OFFSet?

SCPI Example

:RAD:LTEF:WAV:CCAR:TIM:OFFS 0.1ns

:RAD:LTEF:WAV:CCAR:TIM:OFFS?

Notes

Not used for CW Carrier

Unit in GUI: s

State Saved

Yes

Preset

0.000 us

Min

0.000 us

Max

Minimum (Waveform Generation Length – 1 ns or 10 ms – 1 ns) (us)

Initial S/W Revision

A.14.00

Initial Phase

Sets the initial phase of the carrier.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:INITial:PHASe <integer>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:INITial:PHASe?

SCPI Example

:RAD:LTEF:WAV:CCAR:INIT:PHAS 300

:RAD:LTEF:WAV:CCAR:INIT:PHAS?

Notes

Not used for CW Carrier

Unit in GUI: deg

State Saved

Yes

Preset

0

Min

0

Max

359

Initial S/W Revision

A.14.00

Spectrum Control

This section describes the settings of Spectrum Control.

Pre-Filter Clipping

Set the clipping (limit) level of the I/Q waveform before filtering.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:CLIPping:PRE <real>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:CLIPping:PRE?

SCPI Example

:RAD:LTEF:WAV:CCAR:CLIP:PRE 20

:RAD:LTEF:WAV:CCAR:CLIP:PRE?

Notes

Value is in percent [%], 100 means 100 %

100 % means "no clipping"

Unit in GUI: %

State Saved

Yes

Preset

100

Min

10

Max

100

Resolution

0.1

Initial S/W Revision

A.14.00

Post-Filter Clipping

Set the clipping (limit) level of the I/Q waveform after filtering.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:CLIPping:POST <real>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:CLIPping:POST?

SCPI Example

:RAD:LTEF:WAV:CCAR:CLIP:POST 30

:RAD:LTEF:WAV:CCAR:CLIP:POST?

Notes

Value is in percent [%], 100 means 100 %

100 % means "no clipping"

Unit in GUI: %

State Saved

Yes

Preset

100

Min

10

Max

100

Resolution

0.1

Initial S/W Revision

A.14.00

Auto Symbol Rolloff Length Configuration

Double-click or use the drop-down menu to turn the auto symbol rolloff length configuration on or off.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:SROLloff:AUTO[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:SROLloff:AUTO[:STATe]?

SCPI Example

:RAD:LTEF:WAV:CCAR:SROL:AUTO 1

:RAD:LTEF:WAV:CCAR:SROL:AUTO?

State Saved

Yes

Preset

ON [E-UTRA/eMTC/UPLINK NB-IoT/PRACH NBIoT]

Initial S/W Revision

A.14.00

Modified S/W Revision

A.19.00

Symbol Rolloff Length

The cyclic prefix used with SC-FDMA modulation in LTE results in a discontinuity between SC-FDMA symbols. Windowing is used in the Signal Studio for 3GPP LTE software to reduce spurious signal generation between symbols caused by this discontinuity. Symbol Rolloff sets the windowing length in Basic Time Units. Adjusting the Symbol Rolloff Length can improve ACPR performance, however this may result in degraded EVM performance.

Basic Time Unit (Ts) = 1/(15000 x  2048) seconds

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:SROLloff:LENGth <integer>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:SROLloff:LENGth?

SCPI Example

:RAD:LTEF:WAV:CCAR:SROL:LENG 20

:RAD:LTEF:WAV:CCAR:SROL:LENG?

State Saved

Yes

Notes

Unit in GUI: Ts

Preset

15 Ts [E-UTRA/eMTC]

400 Ts [Uplink NB-IoT/PRACH NB-IoT]

Min

0

Max

400

Initial S/W Revision

A.14.00

Modified S/W Revision

A.19.00

Baseband Filter

Sets the state of the baseband filter on or off. In most testing conditions, Keysight recommends using the baseband filter (Baseband Filter = On) to achieve a balance between ACPR and EVM performance.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:BFILter[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:BFILter[:STATe]?

SCPI Example

:RAD:LTEF:WAV:CCAR:BFIL ON

:RAD:LTEF:WAV:CCAR:BFIL?

State Saved

Yes

Preset

ON [E-UTRA/eMTC] [Basic Downlink] [PRACH NB-IoT]

OFF [Uplink NB-IoT]

Initial S/W Revision

A.14.00

Modified S/W Revision

A.19.00

ACP Optimized Filter Type

[Uplink NB-IoT]

Choices: Standard | Narrow | Custom

Default: Standard

Narrow filter provides better spectrum performance, but EVM may degrade.

This setting is available when Baseband Filter is set to ON.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<channel>:ACPFILTer:TYPE STANdard|NARRow|CUSTom

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<channel>:ACPFILTer:TYPE?

SCPI Example

 

State Saved

Yes

Preset

STANdard

Initial S/W Revision

A.19.00

Carrier Aggregation

The Carrier Aggregation node holds the settings of carrier aggregation.

Auto Carrier Aggregation Configuration

Sets the state of Auto Carrier Aggregation Configuration on or off.

Frequency Offset and Cell ID are always editable, even if Auto Carrier Aggregation Configuration is on.

In either case below (1 or 2), auto configuration is performed for Frequency Offset and Cell ID.

  1. When any of these actions are performed: Add Carrier, Delete Carrier or Change System BW, and the Auto Carrier Aggregation Configuration parameter is on.

  2. When the Auto Carrier Aggregation Configuration parameter is changed from off to on.

Auto configuration sets Cell ID same as Component Carrier Index.

If Auto Carrier Aggregation Configuration is set to off, auto configuration does not work.

Frequency Offset of NB-IoT carrier is not automatically set by this parameter.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:CAConfig:AUTO[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:CAConfig:AUTO[:STATe]?

SCPI Example

:RAD:LTEF:WAV:CCAR:CAC:AUTO OFF

:RAD:LTEF:WAV:CCAR:CAC:AUTO?

Dependencies

This setting affects all carriers in the same carrier aggregation group

Changing the state of one carrier to on also changes the state of other carriers in the same carrier aggregation group so that all carriers have the same value.

State Saved

Yes

Preset

ON

Initial S/W Revision

A.14.00

Primary Cell

Sets the primary cell (PCell) in active component carriers.

The primary cell is only one in the component carriers.

Component carriers are composed of the primary cell and all secondary cells.

If the component carrier for the primary cell is deleted or its state is changed, a suitable component carrier for the primary cell is automatically set by the software.

See 3GPP TS 36.331 for more information.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PCELl[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PCELl[:STATe]?

SCPI Example

:RAD:LTEF:WAV:CCAR:PCEL ON

:RAD:LTEF:WAV:CCAR:PCEL?

Dependencies

Only one carrier in a carrier aggregation group can be a primary cell

At least one carrier must be turned on

Turning on this setting on one carrier turns off the setting of other carriers in the same carrier aggregation group

State Saved

Yes

Preset

On (at the first carrier in a carrier aggregation group), otherwise Off

Initial S/W Revision

A.14.00

Carrier Common

Carrier Assignment ARB

Carrier Settings Real-Time

Welcome to LTE FDD